{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can the wire binding screws from a PK ground kit (like PK15GTA or PK23GTA) be used as a replacement screw for the Homeline branch neutral bar?

Issue:

Can the wire binding screws from a ground kit (like PK27GTA) be used as a replacement for the Homeline branch neutral bar?

Product Line:

Homeline Load Centers

Resolution:

Yes, the wire binding screws from the PK ground bar kits can be used as a replacement wire binding screw for the Homeline branch neutral bars, because they are the same screw.

Schneider Electric USA

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: