EcoStruxure Building Commission
The EcoStruxure Building Commission mobile application is designed to improve the commissioning processes by providing users access to SpaceLogic IP Controllers and peripheral I/O devices directly via their mobile devices.
EcoStruxure Building Commission allows for:
Reduced commissioning time: Does not require an EcoStruxure BMS server to be present in the system. Users can get started configuring controllers as soon as they are powered.
Simplified workflows: Provides users with the exact tools they need to carry out their tasks.
Direct configuration and programming: Users can configure settings, upgrade firmware, and load applications directly to their SpaceLogic IP Controllers.
Report generation and status check: Users can generate and view input & output reports, balancing reports, and diagnostic reports as well as check status of the progress.
Elimination of dependencies: Allows for projects to work around obstacles, and eliminate dependencies on network infrastructure.
There are two ways to connect EcoStruxure Building Commission mobile application to SpaceLogic IP Controllers:
Bluetooth - The EcoStruxure Building Commission mobile application can connect to a single SpaceLogic IP Controller via the SpaceLogic Bluetooth Adapter (which is directly connected to a SpaceLogic Sensor) or directly to an RP-C/RP-V controller via its onboard Bluetooth capability.
EcoStruxure Building Commission allows for:
Reduced commissioning time: Does not require an EcoStruxure BMS server to be present in the system. Users can get started configuring controllers as soon as they are powered.
Simplified workflows: Provides users with the exact tools they need to carry out their tasks.
Direct configuration and programming: Users can configure settings, upgrade firmware, and load applications directly to their SpaceLogic IP Controllers.
Report generation and status check: Users can generate and view input & output reports, balancing reports, and diagnostic reports as well as check status of the progress.
Elimination of dependencies: Allows for projects to work around obstacles, and eliminate dependencies on network infrastructure.
There are two ways to connect EcoStruxure Building Commission mobile application to SpaceLogic IP Controllers:
- IP Network - setting up a Wi-Fi access point or direct connection to your network, you will be able to connect your mobile device with all SpaceLogic IP Controllers on your local wireless network.
Size | iOS: 218,55 MB / Android: 35,65 MB |
Price | Free |
Languages | English, Chinsese (Simplified), Czech, Danish, Dutch, Finnish, French, German, Italian, Norwegian, Polish, Portuguese, Russian, Slovenian, Spanish, Swedish |
Scan QR codes with your phone