An arc flash is an electrical accident that creates a dangerous, high-temperature explosion.
An arc flash results from an arc fault. Arc faults are caused by electricity discharging between two or more conductors that are improperly connected, such as frayed wires. Dust or moisture can also cause arcing between conductors, which explains why high-voltage power lines will glow in foggy weather.
Use this Arc Flash library to learn:- Why an electrical arc flash happens
- Steps for arc flash protection
- How to optimize safety and reliability in your facility’s power system
Get expert tips on arc flash mitigation in our free white paper
Arc flash events can result in significant injury to workers. Learn how the most effective arc flash safety programs are those that look to incorporate “safety by design” and other techniques.
Why Is An Arc Flash Dangerous?
In power systems with improper arc flash protection, when a person gets too close to a live conductor, the current can escape its conductor, travel across dusty or moist air, and reach the nearby person. Flipping an improperly configured switch can also cause an arc flash. These are just a couple possible reasons why an arc flash could occur.An arc flash is dangerous: It can vaporize surrounding metal, set fires, create deafeningly loud noises, and result in severe burns. Although rare, arc flashes can have grave consequences. That’s why you need to ensure your people and site are always protected against an arc flash.
What Is the Goal of Arc Flash Protection?
The goal of arc flash protection is to reduce the amount of personal protective equipment (PPE) and potential arc flash energy to levels that allow tasks to be performed on equipment in a smooth and unobtrusive manner. PPE includes rubberized clothing that does not conduct electricity.An electrical arc flash can happen at any time during your power equipment’s lifecycle. Abnormal conditions, such as improper installation, excessive impurities, or failing equipment will increase the risk. One of the critical steps for optimizing safety is to use proper PPE. Aside from the danger, an arc flash can also render equipment unusable and force extended downtime with serious financial consequences. PPE helps avoid bodily harm, but it does not prevent equipment damage. This leads to the question of how to prevent an arc flash in the first place.Schneider Electric offers a number of arc flash mitigation solutions that make this possible, including switchgear, software, and circuit breakers for both passive and active arc flash protection. Our systems work in compliance with the National Fire Protection Association (NFPA) 70E: Standard for Electrical Safety in the Workplace.
MCC Arc Flash Test: Side-By-Side Event
ArcBlok™ is designed with features that help avoid an arc flash before it happens.
Electrical Arc Flash Prevention e-Learning Module
Electrical Safety TrainingElectrical Safety Awareness for Non-Electrical Workers
Learn ways to check and improve safety knowledge when working around electricity on the job.
White papers are provided in .pdf format.
Learn about electrical safety training courses with our e-learning, practical, and hands-on offer.
Blogs, presentations, and more.
Arc Flash Safety Products
- Model 6 AR Motor Control Center by Square D™

Model 6 AR Motor Control Center by Square D™
Model 6 AR Motor Control Center by Square D™ Power-Zone 4 Arc Resistant 
Power-Zone 4 Arc Resistant
Power-Zone 4 Arc Resistant Motorpact Medium Voltage Controllers 
Motorpact Medium Voltage Controllers
Motorpact Medium Voltage Controllers Switchboards and Switchgear 
Switchboards and Switchgear
Switchboards and Switchgear Circuit Breakers 
Circuit Breakers
Circuit Breakers PowerLogic™ P5 Protection Relays 
PowerLogic™ P5 Protection Relays
PowerLogic™ P5 Protection Relays PowerLogic™ P3 Protection Relays 
PowerLogic™ P3 Protection Relays
PowerLogic™ P3 Protection Relays
Access FREE, customized expertise in your Electrical Contractor Portal
Connect for exclusive resources, technical support, and more to grow your business.