Our Brands

Schneider Electric USA Website

Welcome to our website.

Power outages caused by extreme weather events have seen a significant increase, with a reported spike of 67% according to a study by Climate Central. These occurrences have underscored the need for reliable backup power supplies to ensure continuous operation of mission-critical facilities, businesses, and homes during such outages. Emergency generators play a crucial role in providing backup power, but connecting them effectively to the equipment they serve requires the use of transfer switches.

Definition
A transfer switch is a device designed to transfer electrical loads between power sources, such as utility power and generator power. During a power outage, it is utilized to connect electrical loads to a backup power source, typically a generator. Depending on the selected transition mode , the transfer switch can facilitate this transfer without impacting downstream equipment or by introducing a strategic delay. Additionally, transfer switches prevent generators from back-feeding power into the grid, promoting safety objectives.

Incorporating transfer switches into electrical systems helps ensure compliance with relevant electrical codes and standards. For instance, the National Electric Code® mandates the use of a permanent switching means to connect a contingent power source in establishments with a single generator. When coupled with a connection panel, this best practice allows for the reliable provision of temporary power to homes and businesses during emergency situations, enabling quick connections and minimizing downtime.

Transfer switches find application in various settings, making them a versatile device in electrical power distribution. They can be integrated into the following environments:

Data Centers
Transfer switches are essential in data centers to ensure uninterrupted power supply, protecting critical servers and equipment from outages.

Commercial Buildings
Businesses heavily rely on continuous power for their operations. Transfer switches enable a seamless transition to backup power, avoiding disruptions and potential financial losses for business owners that are operating in commercial buildings .

Small Businesses
Even smaller establishments require backup power solutions to safeguard against power outages. Transfer switches enable efficient power transfer, ensuring essential systems and equipment remain operational.

Hospitals
Uninterrupted power is of utmost importance in medical facilities. Transfer switches facilitate a swift transfer to backup power sources in hospitals , preserving the operation of critical medical equipment and life support systems.

Residences
Homeowners can benefit from transfer switches, which provide a reliable connection between generators and essential household equipment during power outages.

Water Treatment Plants
Continuous power is crucial for water treatment plants to maintain essential operations. Transfer switches ensure a seamless transition to backup power sources, preventing interruptions in the treatment process.

Telecommunication Facilities
Transfer switches play a vital role in telecommunications to ensure uninterrupted communication services during power outages.

The operation of transfer switches is relatively straightforward. These devices are installed between a building's power distribution system and its power sources. Their purpose is to transfer the electrical load of a facility between power sources, thereby connecting an active source of power. This is achieved through a mechanism within the switch that disconnects the electrical load from one source and connects it to another, ensuring a smooth transition.

It is important to note that transfer switches should not be confused with circuit breakers. Circuit breakers are designed to protect electrical circuits from overloads by opening to interrupt power flow when overcurrents occur. In contrast, transfer switches are responsible for connecting a power source to a circuit, even when overcurrents up to the device's maximum ratings are present.

Transfer switches are available in different types to suit various needs:

Certain aspects of transfer switch design attract particular attention, resulting in comparisons of modes of operation (Manual vs. Automatic), transition sequences (Open, Delayed, Closed), and special equipment arrangements (Service Entrance, Isolation-Bypass, Custom Engineered). Instead, this document focuses on the most essential functions that all Automatic transfer switches (ATS) must complete to transfer loads without human intervention.

Essential ATS Functions

Regardless of design and feature set, there are specific tasks that an ATS must perform to execute a switching cycle. The tasks required to switch load from a normal power source to an emergency source and back again are explained in the following sections.

Functions and Their Importance

Function 1: Carry Current Continuously

The primary reason why a facility installs a transfer switch is to keep its electrical loads connected to either one of two sources of power. As a result, a transfer switch is designed to remain connected to power distribution circuits under all foreseeable circumstances, including very large fault and short-circuit currents. Conversely, a transfer switch is not designed to protect load circuits and equipment. Rather, overcurrent protection devices open circuits, clear faults, and protect downstream circuits and equipment.

Consider the consequences if transfer switch contacts opened before overcurrent protection devices as the result of a fault current. First, the switch would be isolated from all sources of power immediately following the event. This contradicts the reason for installing an ATS – to maintain power flow to loads. Second, where overcurrent protection devices are selectively coordinated across a power distribution system, the opening of transfer switch contacts could result in power loss to an unnecessary quantity of loads, increasing the impact on facility operations and making recovery more complex. For more information, see the ASCO White Paper entitled Selective Coordination Basics.

For these reasons, an ATS must be able to continuously carry both 100 percent of its rated service current as well as any fault currents that could reach the transfer switch location. In North America and other regions, Withstand Ratings that indicate the fault current capacity are verified by testing transfer switches to requirements of the UL 1008 standard. For more information, see the ASCO White Paper entitled UL1008 Transfer Switch Withstand and Closing Ratings. For Europe and other regions, see IEC Standard 60947-6-1.

Function 2: Detect Power Failures

The capability that differentiates an ATS from non-automatic and manual transfer switches is the ability to self-initiate load transfer when outages of unacceptable power conditions occur. To do so, an ATS must monitor voltage and frequency on the connected power source. When voltage and frequency are out-of-range or absent, a transfer switch will initiate a transfer sequence.

Function 3: Initiate the Alternate Source

In a small minority of installations, an ATS may be used to switch between two sources of power that are expected to always be live, such as between two utility feeds. However, for the vast majority of backup power systems, emergency power will be provided by a genset that is driven by an internal combustion engine that operates only when needed. As such, the engine must be successfully started so that load can be transferred to the gensets they power. To do so, an ATS must issue a start signal to the genset.

Function 4: Transfer Load to the Emergency Source

A genset takes time to start and then accelerate to the operating speed needed to produce acceptable power. The ATS monitors voltage and frequency to verify acceptable power, then transfers load. If the ATS does not detect acceptable power, no transfer occurs because this action would not improve power availability to loads. Doing so would leave loads isolated from the normal source should acceptable power return.

The transfer sequence is determined by the real-time power conditions and the transfer switch’s design. Of note, when an outage of the normal source occurs with a Closed Transition Transfer Switch, transfer from the normal to emergency sources will be an open transition sequence with a momentary power interruption, necessarily so because only the emergency source is live. Later, retransfer to normal will occur without interruption because both power sources are live. Importantly, an ATS needs to complete transfers even under fault conditions because these currents are to be cleared by overcurrent protection devices. For this reason, testing prescribed by listing agencies verifies close-on ratings for transfer switches.

Function 5: Sense Restoration of the Normal Source

While connected to the emergency source, the ATS monitors the condition of the normal source. When acceptable power returns, the transfer switch initiates transfer from the emergency source to the normal source.

Function 6: Retransfer Load to the Normal Source

After sensing restoration of acceptable power, an ATS initiates retransfer to the normal source. In this instance, both power sources are available and acceptable. Typically, retransfer occurs when voltages, frequencies, and (where applicable) phase angles of the two sources are within 5 percent, 2 Hertz, and 5 degrees, respectively. For more information, see the ASCO Power Technologies Basic Power Source Synchronization and Paralleling video and technical brief.

The Role of Delays

The sections above address the essential functions of an ATS and the events that necessarily occur during every switching cycle. Not mentioned are the roles of various delay settings used in conjunction with these operations. For instance, how can an ATS differentiate whether an anomaly on a normal source is merely a short sub-cycle nuisance or a bona fide outage? Use a short delay to verify that the condition is persistent. How can an ATS verify that restored power is stable? Introduce a delay to stay on generator while the ATS controller verifies stable power over a prescribed interval.

ASCO Power Technologies recently explained the role of common delays in another Tech Brief. See Basic Timing Delays For Load Transfer for more information.

Summary

To transfer loads between power sources, automatic transfer switches must (1) carry current continuously, (2) detect power failures, (3) initiate the alternate source, (4) transfer load to the emergency source, (5) sense restoration of power to the normal source, and (6) retransfer load to the normal source. Importantly, an ATS must be able to carry any fault currents that could reach the transfer switch location so that faults can be cleared by overcurrent protection devices designed for that purpose. For more information, review the resources referenced above or contact an ASCO Power Technologies representative.

Manual

Manual transfer switches remain connected to one power source until someone operates it to connect the alternate source. It requires a qualified individual to recognize an outage before operating the device to transfer loads from one power source to another. Manual transfer switches offer simple cost-effective solutions for applications that can tolerate momentary power interruptions.

Automatic

Automatic transfer switches offer unattended operation. They detect power failures, initiate generator startup, transfer load, and perform other functions without human intervention. They also return loads to the normal power source after power returns

Non-Automatic Transfer Switches

Similar to manual transfer switches, non-automatic switches require a qualified person to operate them. However, they can be controlled using local or remote controls. This feature enables the operator to manage the transfer switch from a safer location, making the operation more convenient and user-friendly compared to manual transfer switches.

In conclusion, transfer switches play a critical role in ensuring seamless and reliable power transfer between different sources, particularly during power outages caused by extreme weather events. Their integration into electrical systems helps comply with electrical codes and standards while enabling uninterrupted operation of essential equipment and systems. Whether in data centers, commercial buildings, hospitals, or residential settings, transfer switches provide a vital link between power sources and the equipment they serve, minimizing downtime and ensuring continuous power supply.

Reference:
1. Power OFF: Extreme Weather and Power Outages. (2020, September 30). Climate Central.
https://medialibrary.climatecentral.org/resources/power-outages. Accessed September 2, 2021.

Ready to learn more about Transfer Switches? Find related resources here:

Engineers planning together

Benefits of Custom-Engineered Transfer Switches

Learn about the benefits of custom-engineered transfer switches.
An earthquake hazard map

Seismic Options for ASCO Transfer Switches

Learn about the Seismic Options for ASCO Transfer Switches
A transfer switch facility

Explore ASCO’s Transfer Switches

Waste water treatment plant

Wastewater Treatment Plant

Learn how ASCO provided ATS solutions to a Wastewater Treatment Plant in Glasgow, Montana, USA.

Need help?

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Start your sales inquiry online and an expert will connect with you.

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Find support resources for all your needs, in one place.

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.