Our Brands

Schneider Electric USA Website

Welcome to our website.

When to Separately Ground a Backup Generator

Automatic Transfer Switches (ATSs) are available with and without provisions for switching the neutral conductor. These options accommodate backup power systems where a generator’s neutral conductor is grounded either (1) to the grounding conductor that leads to the facility’s grounding electrode near its service entrance, or (2) a separate grounding electrode near the generator. This article summarizes when a separate grounding electrode is needed.

The Need for Ground Fault Protection

In evaluating grounding schemes and transfer switch designs, it is useful to first understand the need for ground fault protection. A ground fault is an inadvertent current pathway that develops between an energized conductor and an equipment frame or earth. If the fault energizes equipment surfaces that people can touch, it poses an electrical safety hazard. If an arcing ground fault persists at a level below the amount of current that would open a fuse or circuit breaker, it could also pose a fire hazard. To mitigate hazards, Article 230.95 of the National Electrical Code® (NEC®) states:

“Ground-fault protection of equipment shall be provided for solidly grounded wye electric services of more than 150 volts to ground but not exceeding 1000 volts phase-to-phase for each service disconnect rated 1000 amperes or more.”

A common scheme for detecting ground faults is to use a current transformer(s) to monitor current flow through a circuit’s phase and neutral conductors, as shown in Figure 1. If the sum of current flow is other than zero, a ground fault is indicated. In that event, the ground fault sensing equipment signals a device to open the circuit to mitigate hazards.

Controlling Current Pathways

Accurate ground fault sensing requires that the current pathways are known. For instance, if a power system used two grounding electrodes simultaneously without other provisions, some current could return through earth without passing through ground fault sensing equipment, as shown in Figure 2. This would cause sensing equipment to falsely detect faults, causing nuisance tripping and affecting system reliability and availability.

For this reason, a switched neutral can be used in the ATS to isolate the neutral of the unconnected power source. This is the arrangement shown is Figure 1.

Key Electrical Code Requirements

Article 250.20(B) of the 2020 NEC sets forth requirements for grounding alternating current systems where transformers supply 50 to 100 Volts. In addition, Article 250.30 sets forth requirements for grounding separately derived systems, which is first defined in Article 100 as follows:

Separately Derived System.
An electrical source, other than a service, having no direct connection(s) to circuit conductors of any other electrical source other than those established by grounding and bonding connections.

Thus, where a backup generator neutral conductor is grounded to a dedicated nearby electrode, it forms a separately derived system. As such, Article 230 goes on to state:

250.30 Grounding Separately Derived Alternating-Current Systems.
In addition to complying with 250.30(A) for grounded systems, or as provided in 250.30(B) for ungrounded systems, separately derived systems shall comply with 250.20, 250.21, 250.22, or 250.26, as applicable.

Consequently, separately derived systems are those that are not connected to the primary electrical service, and thus require a dedicated grounding electrode.

Following Article 250.30, the NEC provides an informational note that bears on the application:

Informational Note No. 1: An alternate ac power source, such as an on-site generator, is not a separately derived system if the grounded conductor is solidly interconnected to a service-supplied system grounded conductor. An example of such a situation is where alternate source transfer equipment does not include a switching action in the grounded conductor and allows it to remain solidly connected to the service-supplied grounded conductor when the alternate source is operational and supplying the load served.

Consequently, where a generator neutral is bonded to the neutral of the electrical service of a building, the entire system is considered to be singular, not separately derived, and could use a single grounding electrode.

Transferring between Two Neutral Conductors

When the generator neutral is bonded to the service neutral, these conductors are solidly connected at the transfer switch, which switches only the phase conductors. This is the typical configuration of standard transfer switch models.

For separately derived systems, manufacturers also offer transfer switches that switch the neutral conductor together with the phase conductors. Using a switched neutral isolates the ground conductor of the unconnected power source to avoid ground current pathway problems. Again, a switched neutral is shown in Figure 1.

Key Indicators

Viewing all of the prior information in context, systems in the range of 150 to 1000 volts exceeding 1000 Amps require ground fault sensing. Proper sensing will commonly require a dedicated ground at the generator and a switched neutral at the transfer switch.

For applications below 1000 Amps where a generator neutral is grounded back to the service entrance, only one grounding electrode is used. This requires a transfer switch with solid neutral connection. However, designers may need to consider other factors to confirm whether to ground the generator directly. Two of them are identified below:

  • If a system below 1000 Amps is being fitted with backup power because it serves a mission-critical function, would ground fault protection be advantageous to the application? If yes, then a separately derived system may still be warranted and a switched neutral transfer switch may be used.
  • If the generator is located far from a service entrance, it may be desirable to install a dedicated grounding electrode near the genset to avoid energizing a long conductor during a fault. In addition, a cable cut along the length of the grounding conductor could leave a running generator ungrounded, resulting in unsafe conditions. Designers might consider using a dedicated grounding electrode near the generator to avoid these conditions. Again, a separately derived system may be warranted and a switched neutral transfer switch may be used.
Closing

The information herein illustrates the most basic factors involved in deciding how to ground a genset. In practice, grounding issues, grounding and ground fault system designs, and the responding codes can be far more complex. Situations requiring special consideration include applications with multiple transfer switches, multiple gensets, lightning protection systems, and mobile or portable generators. Qualified electrical professionals should be used to evaluate grounding needs and specify responding designs. Further information can be reviewed in the references that follow. Representatives of ASCO Power Technologies can be consulted to obtain supporting information for specific applications.

References

National Fire Protection Association: NFPA 70 - National Electrical Code
ASCO Tech Brief: Managing Ground Faults in Backup Power Systems
ASCO White Paper: Switching the Neutral Conductor

Need help?

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Start your sales inquiry online and an expert will connect with you.

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Find support resources for all your needs, in one place.

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.