{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
You are currently viewing the content available in Vietnam. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the lithium battery life expectancy in a XBTGT or XBTGK.
Lithium battery's life expectancy for the XBTGT and XBTGK is:
  1. 10 years when the battery's ambient temperature is less than or equal to 40 deg C (104 deg F)
  2. 10 years when the unit's ambient temperature is less than or equal to 25 deg C (77 deg F)
When used for backup (without main power):
  1. Approximately 60 days, with a fully charged battery
  2. Approximately 6 days, with a 10% charged battery

Schneider Electric Vietnam