What is the difference between LX1 and LX9 coil?
Issue:
LX1 and LX9 characteristic

Product Line:
Tesys F line Contactors and Accessories

Environment:
TeSys™ F AC Coils

Resolution:
The LX1 is the standard control type coil. The LX9 low sealed consumption coil offers high tolerance to inrush voltage drops, immune to micro-breaks (main supply or contact chain) and are capable of operation on networks with harmonic numbers less than or equal to 7.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: