Will the current version of Power Suite Software work with older ATV58 drives?
Issue:
N/A

Product Line:
Altivar Machines, Altivar 58

Environment:
All

Cause:
N/A

Resolution:
Yes, the current version should be able to set any setting in your existing drive.

It will not be possible to use features that are available in the software that are not part of the drive.
For example, one could not assign a logic input to an external fault contact on a drive with version 4.1 firmware. It may show up as an option on Powersuite, but it is not a feature that was available with version 4.1 or older drives.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: