What is the enclosure IP rating for the ATS48 Remote Keypad Mount Kit?
Issue:
Remote Keypad Mount Kit Enclosure IP rating for the ATS48.

Product Line:
Altistart 48

Environment:
All

Cause:
Need enclosure IP rating

Resolution:
The VW3G48101 remote mount keypad kit is incorrectly listed in the Instruction Bulletin 30072-450-61 (06/2002) page 19 as rated IP65. The pricing guide and the catalog both list it correctly as IP54.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: