What is the operating temperature rating of the ATS48?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Where can I find information on Ambient Air Operating Temperature rating of the ATS48?

Product Line:
Altistart 48

Cause:
Selection Criteria Environmental

Resolution:
14 to +104 *F (-10 *C to +40 *C) without derating.
Up to +140 *F (+60 *C), derate the current by 2% for each *C above 40 *C.
14 to 122 *F (-10 *C to +50 *C) with user provided shorting/bypass contactor
Visit -  http://www.altivardrives.com   Scroll down to Altistart Softstarts > Altistart 48 > ATS48 Installation Manual

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: