What size knock outs are provided with the GV2MC01 or GV2MC02 enclosure?
Issue:
GV2MC01 or GV2MC02 cable entry sizes

Product Line:
Tesys GV Manual Starter and Protectors enclosures

Environment:
PowerPact™ Manual Starters

Resolution:
Each enclosure has a total of four knockouts.  There are two concentric knockouts on top and  and two knockouts on the bottom.
Each knockout has an IP20 (20 mm) or IP25 (25 mm) hole available.

Schneider Electric Việt Nam

Phần đính kèm
GV2MC0 outline.JPG.jpg [52.4 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: