What is the part number for Devicenet Option on ATS48 Softstarter?
Issue:
Is Devicenet option available on ATS48 Softstarter?

Product Line:
ATS48, Altistart 48

Environment:
All

Cause:
NA

Resolution:
There is no Devicenet option card for ATS48. The built-in Communication option is Modbus.
However, part number LUFP9 Gateway is available.
The LUFP9 does require set up as it is not specific for the Altistart 48 product.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: