Which ATV71 encoder card would be used with a differential line driver encoder?
Issue:
ATV71 encoder card used with a differential line driver encoder

Product Line:
Altivar 71, ATV71

Environment:
All

Cause:
N/A

Resolution:
The RS422 Encoder interface card would be used.
If required 5v, it would be VW3A3401.
If required 15v, it would be VW3A3402.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: