What relay should be used to provide two wire control for the Class 8903 Type PB lighting contactor?
Issue:
Two wire control relay for the Class 8903 Type PB lighting contactor

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Lighting Contactors

Cause:
Two wire control relay needed

Resolution:
Use any 2 pole relay with a Normally Open and Normally Closed contact, such as
CA2SK11**
8501XO11V**

Complete the part number by adding the appropriate voltage code.  i.e 8501XO11V02 for 120VAC, or CA2SK11G7 for 120VAC.

Schneider Electric Việt Nam