Where is the auxiliary contact located on the Class 9065 Motor Logic solid state overload relay ?

Issue:
How to locate the auxiliary contact on the Class 9065 Motor Logic solid state overload relay.

Product Line:
Class 9065 Motor Logic SSOLR

Environment:
North American Products

Resolution:
The auxiliary contact is mounted left of the adjustment dial in upper left corner of relay. Terminals are marked 95 & 96. Service bulletin 30072-013-33 shows the 9999AC04 contact kit position.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: