Can an auxiliary contact be added to the VC_GU non-metallic enclosed Vario load break switch?
Issue:
Vario auxiliary contact can be added to the VC_GU?

Product Line:
UL 508 Motor Disconnect Switches

Enviroment:
Mini-Vario and Vario™ Assembled and Enclosed Switches

Resolution:
Yes, however this will require removing one of the two grounding straps provided inside the enclosure box to allow room for mounting the auxiliary.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: