undefined [object Object]
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
How many drive configuration files can be stored in the ATV71 keypad?
Issue:
Storing drive configuration files in the ATV61 / ATV71 keypad.

Product Line:
ATV61 ,ATV71

Environment:
All

Cause:
Ffiles stored in keypad

Resolution:
The keypad can store up to 4 files.
To access and manage these files: Go to menu 1.12 (FACTORY SETTINGS) (FCS-)
See programming manual for details, if needed.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: