Are explosion proof enclosures available for GV manual motor starters.
Issue:
NEMA 7/9 rated enclosure for GV manual motor starters

Product Line:
Tesys GV Motor Starters and Protectors

Environment:
TeSys™ GV Manual Starters and Protectors

Resolution:
No hazardous duty enclosures are available for the GV product line.
For explosion proof applications consider the Class 2510 Type M or Type T offering.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: