What is the clear plastic guard that goes on the 9001K1L series illuminated pushbuttons?
Issue:
Replacement clear guard for 9001K1L and 9001SK1L illuminated buttons

Product line:
Push Buttons and Operator Interface

Environment:
9001 Type K and SK Harmony 30mm

Cause:
Replacement parts

Resolution:
The clear plastic guard that goes on top of the illuminated operators is part number 4487D63X1.

Note the past Digests show an error of 4487D63XI.  The correct number is 4487D63X1

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: