Are the auxiliary contacts, Class 9999SX##, for the NEMA 8502 and 8536 contactors and starters rated for DC voltage?
Issue:
DC ratings for Nema aux contact

Product Line:
NEMA Contactors and starters

Environment:
Auxiliary Contacts

Resolution:
The 9999SX series auxiliary contacts are rated for AC voltage only.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: