Tìm các câu hỏi thường gặp
Will the GV2 busbar accessories work with the U-line starters?
Issue:
GV2 busbar U-line compatibility
Product Line:
Contactors and Starters-IEC
Environment:
TeSys™ GV Manual Starters and Protectors
Resolution:
Yes as long as the incoming line barrier, LU9SP0 on the Uline is not required. See the attached catalog page from document 8502CT0201 for details.
GV2 busbar U-line compatibility
Product Line:
Contactors and Starters-IEC
Environment:
TeSys™ GV Manual Starters and Protectors
Resolution:
Yes as long as the incoming line barrier, LU9SP0 on the Uline is not required. See the attached catalog page from document 8502CT0201 for details.
Đã phát hành cho:Schneider Electric Việt Nam
Phần đính kèm
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: