What is Form Y35 for a NEMA starter or contactor or overload relay?
Issue:
Form Y35 for a NEMA starter or contactor or overload relay

Product Line:
NEMA Type S Motor Starters (8536 8736 8606)

Environment:
NEMA Starters

Resolution:
Form Y35 was a catch-all form for special features for which there was no existing form number. It required a description ( ie. Form Y35( for ...... ) ) and engineering approval. In mid 2008 , the Form Y35 for these product lines was discontinued and an SPL or Special was created through Product Selectors for less common modifications for new products .

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: