What is the difference between LAD703 and LA7D03
Issue:
Identifying differences between two similar part numbers

Product Line:
IEC contactors and starters

Environment:
Products sold and used in the United States

Cause:
Identifying differences between two similar part numbers

Resolution:
Both will remotely stop (trip) or electrically reset the overload, however;
LAD703 is used on Tesys overload LRD01 through LRD35 and LR3D01 to LR3D35.
LA7D03 is used on all other LR*D overload relays other than LRD01 to LRD35 and LR3D01 to LR3D35.*

*LR9D01-LR9D32 electronic overload relays do not currently have a remote reset module accessory

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: