What is the part number for door screws on the E-Flex drives?

Issue:
Part number for door screws on the E-Flex drives

Product Line:
ATV61

Environment:
Econo-Flex

Cause:
n/a

Resolution:
The door screw for the E-Flex will fit the Econoflex as well. There is also a retaining washer that is useful to have.

The part numbers and pricing are as follows per Pam Welborn in Seneca.

22906-00003 Screw - Thumb, Stainless $29.52 List Price PE4 Discount
29416-61501 Washer - Retaining $1.00 List Price PE4 Discount

Need to force the order on Seneca.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: