What needs to be done when prompted PrtF Fault on ATV61 display after installing replacement MCB and/or Power Board?

Issue:
ATV61 Drive Shows PrtF Fault after replacing MCB and/or Power Board.

Product Line:
Altivar 61

Environment:
All

Cause:
Altivar 61 with PrtF Fault

Resolution:
Need to Hit Enter, select Power ID (For 18-Pulse CPD=IP00, E-Flex =IP00, MCC = IP00,M-Flex =IP00, Open or Custom Enclosed units = IP20, etc.) Set for IPxx and hold Ent key for 2 seconds.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: