What is the UL listed SCCR rating of a D10 disconnect switches?
Issue:
SCCR for D10 disconnect switch

Product Line:
NEMA Style Door-Mounted Disconnect Switches

Environment:
NEMA Style Disconnect Switches

Resolution:
D10S1 and D10S1H - 5,000 Amperes unless used with Class R or J fuses
For D10S3/D10S3H and D10S4/D10S4H - 10,000 Amperes unless used with Class R or J fuses

NOTE: D10 Disconnect switches have already been discontinued. Contact Technical support for replacement.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: