What is the part number for the front cover (4X7 segment display), on the ATV61/ATV71 drives?
Issue:
Wondering what is the part number for the front cover (4X7 segment display), on the ATV61/ATV71 drives?

Product Line:
ATV61 ATV71

Environment:
All Main control board covers

Cause:
Replacement parts

Resolution:
VX4A1103 was the part number, but has been is obsoleted and no longer available.  Must purchase the entire Main control board, to get the front cover.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: