What class overload protection does the ATV312 drive provide?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
ATV312 overload protection class

Product Line:
Altivar 312

Environment:
Overload protection

Cause:
n/a

Resolution:
The drive provides class 10 overload protection.
You can set this overload parameter in the SEt menu under ITH, which is based on the motor's FLA setting stamped on the motor name plate.
There is additional information in the ATV312 Programming manual.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: