What are the pinouts for the Output Relay on the Environmental Monitoring Unit (AP9319) and the Environmental Management System (AP9320)?


Below are the pinouts:


Pin #

Description

1

No Connection

2, 3

Normally Closed (NC) Contact

4, 5

Common

6, 7

Normally Open (NO) Contact (recommended connection)

8

No Connection


Relay ratings: 1A, 30V AC/DC



Since the user interface allows for either 'normally open' or 'normally closed,' APC recommends using only the normally open contacts and configuring the 'normal' state in the user interface.



Schneider Electric Việt Nam

Tìm hiểu thêm
Danh mục:
Bài viết có thể hữu ích
Tìm hiểu thêm
Danh mục: