Tìm các câu hỏi thường gặp
AP8XXX Series Rack PDU Power Output Specifications (CAN & USB ports)
Issue
This article will review the power output capabilities for the CAN and USB ports on an AP8XXX series Rack PDU.
Product Line
- Rack Power Distribution (PDU) Models
- AP84XX
- AP88XX
- AP89XX
- AP86XX
Environment
- All serial numbers
- All firmware versions
Cause
Information is provided for reference only.
Resolution
Below is a diagram of the current AP8XXX series Rack PDU display for reference:
Item Number | Description | Maximum Output Power |
7 | CAN Bus Ports (for Network Port Sharing use only) | 200mA @ 24VDC nominal (4.8 watts) |
8 | USB Port - (for USB drive to upgrade PDU firmware only) | 100mA @ 5VDC nominal |
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: