Material Safety Data Sheets (MSDS) for Symmetra PX2 and PX 250-500kw UPS

Article available in these languages: Tiếng Tây Ban Nha

Issue:
MSDS information for various battery manufacturers utilized in Symmetra PX2 and PX 250/500 UPS systems

Product:
Symmetra PX2, Symmetra 250-500

Environment:
All models/ All serial numbers


Resolution:
The rules regarding MSDSs changed in 2016 and it’s no longer sufficient just to post a link to the battery MSDS that we use.  When the rules changed, we began authoring Safety Data Sheets (new name for MSDSs) that would meet the new regulations.  These newly authored Safety Data Sheets (SDS) are located at the following web page.

http://www.apc.com/us/en/who-we-are/sustainability/battery-safety/battery-compliance.jsp

You’ll note changes –
Safety Data Sheets are region specific.  There is a NAM format and an EU format.

The intent is to direct all customers to this location when they have SDS or MSDS questions.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: