Halon and FM 200 Leakage and Detection

"NetBotz appliances with the use of third party 4-20mA sensors can be used for detecting leakage of FM-200/Halon.

The following third party sensor will work with the NetBotz 4-20mA pod. Newer NetBotz that do not work with this pod may also have a 4-20 input directly on the device itself.:

The SSG-MCD Suppression System Guard

This system detects Halon1301 and FM-200 fire suppression agents and optionally it can be built with 4-20mA output.

SSG-MCD User's Guide (see page 8)
"

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: