Netbotz | Particle Sensor 120 Specifications
Issue:
Particle Sensor 120 Specifications

Product Line:
NetBotz

Environment:
NetBotz particle sensor NBES0201

Cause:
Sensor specifications.

Resolution:

Particle Sensor Specifications
  • Measures presence of dust, *smoke, or other particulates in sensitive equipment spaces
  • Measures particle concentrations as small as 1 micron
  • Set thresholds on particulate levels, graph past sensor readings
* please note this unit is not meant to be used as a smoke detector.

Placement
  • On floor near equipment or mount on wall
  • Particulates most dense at lower heights, so place as low as possible
Other
  • Periodic lens cleaning required
  • Supported on WallBotz 500 onlyConnects to DIN connector on WallBotz 500 Sensor Pod

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: