NetBotz | Can I calibrate sensors?
Issue:
Sensors values may appear to be off and needing calibration.

Product Line:
NetBotz v2 (320/420/500)
NetBotz v3 (355/356,455/456,450,550,570)

Environment:
Version 2 NetBotz sensors
Version 3 NetBotz sensors

Cause:
Questionable readings from sensors may suggest that devices require calibration.

Resolution:

Sensors (temperature, humidity, airflow, etc.) on version 2 and 3 NetBotz Appliances do not need to be calibrated as they are fully calibrated by the supplier.

If you feel your appliance is not accurately reporting temperature and humidity readings correctly, please contact NetBotz Support.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: