Is it possible to change the lock and key in a NetShelter SX or SV cabinet? Users may want some, or all, their cabinets to be keyed differently.

Issue:
Customers need to know what type of locks are available, how can they be purchased and how they're installed.

Product Line:
NetShelter SX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
A request has been made to replace the existing locks, or to replace the standard locks with uniquely keyed locks.

Resolution:
See Attached

Schneider Electric Việt Nam

Phần đính kèm

20130408 Uniquely Keyed Locks for Netshelter SX Enclosures Rev6.pdf20130408 Uniquely Keyed Locks for Netshelter SX Enclosures Rev6.pdf [356.4 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: