Where are the Model and Serial numbers on the NetShelter SX, SV or VX?
Issue:
Customer cannot find the serial number of the NetShelter cabinet.

Product Line:
NetShelter

Environment:
All versions and serial ranges.
Cause:
Need to locate the serial number.
Resolution:
The serial number and model number are located on a label inside the rear doors on the top of the frame. Simply open the rear doors and look up.
See attached file for photos.

Schneider Electric Việt Nam

Phần đính kèm
NetShelter Serial Number Location for SX VX Networking AV VL.ppt [747.5 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: