PowerChute Personal Edition 3.0 un-installation hangs while re-enabling hibernation on Windows.
Issue:
PowerChute Personal Edition 3.0 un-installation hangs while re-enabling hibernation on Windows.

Product Line:
PowerChute Personal Edition 3.0

Environment:
All supported Windows OS

Cause:
If the text on your screen says re-enabling hibernation, this is happening because the USB port cannot be detected by Windows Device Manager. After the system restart, the USB port will work fine.

Solution:

Restart your PC and then try to uninstall PowerChute Personal Edition 3.0.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: