What is the max duty cycle for the ATS01 soft starters?
Issue:
ATS01 duty cycle.
Product Line:
Altistart 01
ATS01
Environment:
Frequent start/stop cycles
Cause:
Overheating
Resolution:

There are several different versions of ATS01.  Each has it's own characteristics.
See below:

ATS01N1...FT
1 second start time, 100 maximum number of starts per hour
5 second start time, 20 maximum number of starts per hour

ATS01N2206 to N222, LU, QN, RT
1 second start time, 100 maximum number of starts per hour
5 second start time, 20 maximum number of starts per hour
10 second start time, 10 maximum number of starts per hour

ATS01N232, LU, QN, RT
1 second start time, 50 maximum number of starts per hour
5 second start time, 10 maximum number of starts per hour
10 second start time, 5 maximum number of starts per hour

ATS01N2... LY, Q THIS VERSION IS NO LONGER AVAILABLE see the ATS22 product family instead
1 second start time, 360 maximum number of starts per hour
12 second start time, 30 maximum number of starts per hour

Schneider Electric Việt Nam

Phần đính kèm
ATS01 cycle Times.pdf [22.28 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: