Is there a way to get more torque out of the motor when running at lower speeds with an ATV312 drive?
Issue:
How to increase the torque out of a motor when running at lower speeds with an ATV312 drive

Product Line:
ATV312

Environment:
All

Cause:
More torque

Resolution:
First, verify that the motor data is correct in the drC menu.  Then set UFt to L.  In the SEt menu, increase UFr to provide higher torque output.


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: