What is the part number of a potentiometer that can be used on Schneider drive?
Issue:
Is there a Potentiometer available for an AC drive?

Product Line:
All Altivar Drives

Environment:
All

Cause:
Customer needs a speed pot for an Altivar drive.

Resolution:
Most of the drives will accept any potentiometer rated between 1k Ohms and 10 k Ohms, 1/2 Watt. See the installation user guide for the specific drive that you are using to determine the specific range that it can use.

Part number ATVPOT25K is a complete 22mm operator with mounting collar and 2.5K ohm potentiometer that has been a standard part number for many years (drawing attached for reference).  However, this part is in the process of being phased out.
The E-Flex, M-Flex and MCC `s all use the ZB5AD922 operator in conjunction with part # 80442-273-02 (2.5k ohm pot)

Suggest using one of the following:
For 22mm
Metal - XB4BD912R10K
Plastic - XB5AD912R10K

For 30mm
Metal - 9001K2108
Plastic - 9001SK2108

Schneider Electric Việt Nam

Phần đính kèm
ATVPOT25K_DWG.pdf [50.27 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: