Tìm các câu hỏi thường gặp
Temperature/Humidity sensor # added or removed
Issue:
Temperature/Humidity sensor # added or removed
Product line:
ACDA901
Environment:
All Serial Numbers
Cause:
An AP9520TH sensor has been detected. An AP9520TH sensor has been removed.
Resolution:
This alarm occurs every time you add or remove a AP9520TH sensor on the a-link bus. Also you can get a removed alarm if the sensor fails or the connection is disconnected.
Đã phát hành cho:Schneider Electric Việt Nam
Phần đính kèm
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: