Can a dynamic braking resistor be installed on an ATV212 or ATV21 drive?

Article available in these languages: Tiếng Thổ Nhĩ Kỳ

Issue:
ATV212 (or ATV21) connection for a DB resistor

Product Line:
ATV21, ATV212

Environment:
All Models and Serial Numbers

Cause:
Installation question

Resolution:
No, you cannot put a braking resistor on an ATV21/212 drive. These drives are not designed to be installed with a braking resistor.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: