What is the hole size of the padlock provision for a GV2P starter?
Issue:
Padlock hole diameter on GV2P

Product Line:
GV2 Manual Motor Protectors

Environment:
All GV2P, rotary handle.

Cause:
n/a

Resolution:
There are provisions for one padlock only, the hole size is approximately 6mm.  You can add a GV2V03 padlock attachment that will allow up to 6 padlocks for Lock out Tag out applications.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: