Where can you find the conduit kit dimensions for the ATV61 and ATV71 drives?
Issue:
Conduit kit dimensions for the ATV61 and ATV71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Accessories for the ATV61 and ATV71 drives.

Resolution:
You can find the dimensions in the manuals linked below:

For ATV61/71 drives 45kW (60HP) and smaller at 230V  AND less than 75kW (100HP) at 460V):
https://www.se.com/us/en/download/document/30072-451-74/

For larger HP ATV61/71 drives:
https://www.se.com/us/en/download/document/30072-451-73/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: