Does Altivar 61 have a battery that backs up the memory?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Wants to know if the Altivar 61 has a battery that backs up the memory.

Product Line:
Altivar 61, ATV61

Environment:
All models in range.

Cause:
Wants to know if the Altivar 61 has a battery that backs up the memory.

Resolution:
Yes, it has the CMOS battery for programming the back-up. Even without the power leads or 24 Vdc, it will save the program.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: