Video: How do you set up reference switching on the ATV212 drives?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Reference switching between VIA and VIB

Product Line:
ATV21 and ATV212

Environment:
All

Cause:
Switching between two analog references VIA and VIB.

Resolution:
Reference switching can be accomplished by programming a logic input R (F112) or RES (F113) to 38.
Program your FNOD as your 1st reference and F207 as your 2nd reference.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: