What is the appropriate replacement for an ATV11 drive?
Issue:
Needs a replacement part number for an ATV11 drive.

Product Line:
Altivar 11

Environment:
All models and serial numbers

Cause:
Determine the replacement for an ATV11 drive.

Resolution:
The recommended replacement for the ATV11 is the ATV12.  Select the ATV12 based on the motor horsepower, rated motor voltage and supply voltage (single or three phase).

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: