What is the maximum distance the motor can be from the ATV61 and ATV71 drive?


Issue:
is there a maximum distance of the cables connected between the drive and motor?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Application notes on motor cable distance.

Resolution:
Length of motor cables from ATV61


Length of motor cables from ATV71

Length of motor cables from ATV71
Length of motor cables from ATV71

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: