Where can the ATV61 BACnet Manual be downloaded?
Issue:
Looking for the ATV61 BACnet Manual

Product Line:
VW3A3315 BACnet card for use with any ATV61 series drive.
VW3A3319 BACnet card for use with any ATV61 series drive.

Environment:
Part number VW3A3315 or VW3A3319, all serial numbers

Cause:
Installation, configuration and programming information needed for an ATV61 drive equipped with a VW3A3315 or VW3A3319 BACnet cards.

Resolution;
The instruction manual for the older VW3A3315 card is bulletin # atv61_BACnet_EN_V1
Link here: https://www.se.com/us/en/download/document/ATV61_BACnet_card_2006/

The instruction manual for the current VW3A3319 card is bulletin # 1765274.
Link here: https://www.se.com/us/en/download/document/1765274/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: