CET850 Error "SFTCommon-ICDLibrary not installed", "SFTCommon-SCLSchema not installed"

Issue:
When attempting to install the CET850 software, the following errors may be seen:
- SFTCommon-ICDLibrary not installed
- SFTCommon-SCLSchema not installed

Environment:
CET850 software

Cause:
Then after installing, when attempting to open the CET850 software, the following message may appear:
- SFTCommon Library is not installed in the system. Please install the SFTCommon Library before starting the CET850 Application.

Resolution:
This can be corrected by downloading and installing SFT2841 (free software):
https://download.schneider-electric.com/files?p_enDocType=Software+-+Release&p_File_Name=setup_SFT2841_17.4.0.exe&p_Doc_Ref=Setup_Software_SFT2841&_ga=2.125571978.1633494616.1675105935-1682550843.1657719175

Installing SFT2841 will install the SFTCommon-ICDLibrary and SFTCommon-SCLSchema.

When asked for a Serial Number for SFT2841, use '0647740-08' or '8888888-06'.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: